modelListener overriding virtual functions from different screens
I have created 2 screens , screen1 and screen2, and I would like to override 2 virtual functions inside the ModelListener class from Screen1Presenter and Screen2Presenter respectively. However the overridden function from the derived classs (i.e. Screen1Presenter and Screen2Presenter) is never called.
I have no idea how to solve this problem because its a weird scenario and I am unsure what to search to solve this problem...
Model.cpp
void Model::myBtn1Clicked(void){
modelListener->ShowScreen2(); ///called successfully
}
void Model::myBtn2Clicked(void){
modelListener->ShowScreen1(); ///called successfully
}ModelListener.hpp
#ifndef MODELLISTENER_HPP
#define MODELLISTENER_HPP
#include <gui/model/Model.hpp>
class ModelListener
{
public:
ModelListener() : model(0) {}
virtual ~ModelListener() {}
void bind(Model* m)
{
model = m;
}
virtual void ShowScreen1(){} //// this line s called , instead of the intended Screen1Presenter::ShowScreen1()
virtual void ShowScreen2(){} //// this line is called , instead of the intended Screen2Presenter::ShowScreen2()
protected:
Model* model;
};
#endif // MODELLISTENER_HPPScreen1Presenter.hpp
#ifndef SCREEN1PRESENTER_HPP
#define SCREEN1PRESENTER_HPP
#include <gui/model/ModelListener.hpp>
#include <mvp/Presenter.hpp>
using namespace touchgfx;
class Screen1View;
class Screen1Presenter : public touchgfx::Presenter, public ModelListener
{
public:
Screen1Presenter(Screen1View& v);
/**
* The activate function is called automatically when this screen is "switched in"
* (ie. made active). Initialization logic can be placed here.
*/
virtual void activate();
/**
* The deactivate function is called automatically when this screen is "switched out"
* (ie. made inactive). Teardown functionality can be placed here.
*/
virtual void deactivate();
virtual ~Screen1Presenter() {};
void myBtnClicked();
virtual void ShowScreen1(void) override;
private:
Screen1Presenter();
Screen1View& view;
};
#endif // SCREEN1PRESENTER_HPPScreen1Presenter.cpp
#include <gui/screen1_screen/Screen1View.hpp>
#include <gui/screen1_screen/Screen1Presenter.hpp>
Screen1Presenter::Screen1Presenter(Screen1View& v)
: view(v)
{
}
void Screen1Presenter::activate()
{
}
void Screen1Presenter::deactivate()
{
}
void Screen1Presenter::myBtnClicked()
{
model->myBtn1Clicked();
}
void Screen1Presenter::ShowScreen1(void){ //NEVER CALLED
view.ShowScreen();
}
Screen2Presenter.hpp
#ifndef SCREEN2PRESENTER_HPP
#define SCREEN2PRESENTER_HPP
#include <gui/model/ModelListener.hpp>
#include <mvp/Presenter.hpp>
using namespace touchgfx;
class Screen2View;
class Screen2Presenter : public touchgfx::Presenter, public ModelListener
{
public:
Screen2Presenter(Screen2View& v);
/**
* The activate function is called automatically when this screen is "switched in"
* (ie. made active). Initialization logic can be placed here.
*/
virtual void activate();
/**
* The deactivate function is called automatically when this screen is "switched out"
* (ie. made inactive). Teardown functionality can be placed here.
*/
virtual void deactivate();
virtual ~Screen2Presenter() {};
void myBtnClicked();
virtual void ShowScreen2(void) override;
private:
Screen2Presenter();
Screen2View& view;
};
#endif // SCREEN2PRESENTER_HPPScreen2Presenter.cpp
#include <gui/screen2_screen/Screen2View.hpp>
#include <gui/screen2_screen/Screen2Presenter.hpp>
Screen2Presenter::Screen2Presenter(Screen2View& v)
: view(v)
{
}
void Screen2Presenter::activate()
{
}
void Screen2Presenter::deactivate()
{
}
void Screen2Presenter::myBtnClicked()
{
model->myBtn2Clicked();
}
void Screen2Presenter::ShowScreen2(void){ //NEVER CALLED
view.ShowScreen();
}I believe i've posted the relevant codes. Please let me know if anything need clarification
Update 1:
I made a cheap work-around by making all the functions static... really hoped the virtual function overload could work...
Model.cpp
#include <gui/model/Model.hpp>
#include <gui/model/ModelListener.hpp>
#include <gui/screen1_screen/Screen1Presenter.hpp> //added
#include <gui/screen2_screen/Screen2Presenter.hpp> //added
Model::Model() : modelListener(0)
{
}
void Model::tick()
{
}
void Model::myBtn1Clicked(void){
Screen2Presenter::ShowScreen2(); //direct call
}
void Model::myBtn2Clicked(void){
Screen1Presenter::ShowScreen1(); //direct call
}
ModelListener.hpp
#ifndef MODELLISTENER_HPP
#define MODELLISTENER_HPP
#include <gui/model/Model.hpp>
class ModelListener
{
public:
ModelListener() : model(0) {}
virtual ~ModelListener() {}
void bind(Model* m)
{
model = m;
}
//virtual void ShowScreen2(){} // REMOVED
//virtual void ShowScreen1(){} // REMOVED
protected:
Model* model;
};
#endif // MODELLISTENER_HPP
Screen1Presenter.hpp
public:
static void ShowScreen1(void);
Screen1Presenter.cpp
void Screen1Presenter::ShowScreen1(void){
Screen1View::ShowScreen();
}
Screen1View.hpp
public:
static void ShowScreen(void);
Screen1View.cpp
void Screen1View::ShowScreen(void){
static_cast<FrontendApplication*>(Application::getInstance())->gotoScreen1ScreenWipeTransitionWest();
}