Skip to main content
JKaz.1
Associate III
January 30, 2026
Question

Need to tell the TouchGFX Designer to stop generating canvas buffers

  • January 30, 2026
  • 1 reply
  • 197 views

Right now, if there are any widgets on a page the Designer automatically creates a canvas buffer for it.  The following code is created in the ViewBase .hpp/.cpp files

static const uint32_t CANVAS_BUFFER_SIZE = 12000;
uint8_t canvasBuffer[CANVAS_BUFFER_SIZE];

touchgfx::CanvasWidgetRenderer::setupBuffer(canvasBuffer, CANVAS_BUFFER_SIZE);

 

This gets set up for each view that has widgets.  I want it to STOP DOING THAT.  I want to allocate my own buffer to it, in a piece of ram that I choose.  Please, please, please give me the option to tell the Designer that I will handle it myself.

I can allocate my own buffer in the TouchGFXHAL::initialize() function, but it's just going to get overridden as soon as a View gets, as that constructor will set up it's own function.

This is especially important, because I have give it a buffer at the start of time anyways, otherwise it crashes.  When the view page is changed to, it calls StatusContainer, which calls an IconContainer, which sets the tint of the icon.  Setting the tint calls VectorRenderer->draw, which is going to use the CanvasBuffer.
Only after all of this is done, is the constructor for ViewBase hit, and the canvas buffer for the page get's initialized.

So, not only am I forced to use the canvas buffer of the page, it is setup too late to actually be useful for that page at initialization time.  Seems like a double flaw.

1 reply

Visitor II
February 3, 2026

I'm interested in that too. My goal is to have one canvas buffer, created in FrontendApplication.hpp, used in all of the screens.

 

Update:

Came up with the following not very elegant solution for now. In the touchgfx project folder made "remove_canvas_buffer.bat" file with the following commands (replace CPP_LINE1_TO_REMOVE, HPP_LINE1_TO_REMOVE, HPP_LINE2_TO_REMOVE with your strings):

set CPP_LINE1_TO_REMOVE=touchgfx::CanvasWidgetRenderer::setupBuffer(canvasBuffer, CANVAS_BUFFER_SIZE);
find ./generated/gui_generated/ -type f -name "*.cpp" | xargs sed -i "s/%CPP_LINE1_TO_REMOVE%//g"

set HPP_LINE1_TO_REMOVE=static const uint32_t CANVAS_BUFFER_SIZE = 19200;
find ./generated/gui_generated/ -type f -name "*.hpp" | xargs sed -i "s/%HPP_LINE1_TO_REMOVE%//g"

set HPP_LINE2_TO_REMOVE=uint8_t canvasBuffer\[CANVAS_BUFFER_SIZE\];
find ./generated/gui_generated/ -type f -name "*.hpp" | xargs sed -i "s/%HPP_LINE2_TO_REMOVE%//g"

Then change Designer -> Config -> Build -> Post Generate Target Command to "touchgfx update_project && remove_canvas_buffer.bat". That way after every code generation the strings CPP_LINE1_TO_REMOVE, HPP_LINE1_TO_REMOVE and HPP_LINE2_TO_REMOVE will be removed in generated code.