Skip to main content
Associate II
October 13, 2025
Solved

New Project 5 months later and the screen is flipped 180??

  • October 13, 2025
  • 6 replies
  • 524 views

I created a simple project back in May (simple - some buttons, temperature display) and mounted in a box (landscape/0 rotation).

I went to reuse the display with a new TouchGFX project (same box) and it is flipped 180! When I load the old code, correct side up, new project in TouchGFX and it is upside down.  

I checked the forum and this isn't easy to do and requires extra code - how is this even possible?  

For reference, it is a fairly new STM32F469I-DISCO (blue) purchased in May of 2025.  Old project - SDCARD/Headphone jack faces down.

Best answer by JohanAstrup

Previously, two TBSs were available in TouchGFX Designer for the STM32F469I-DK. One of these was called STM32F469I-DISCO-REV-AU1 and covered the new revision of the discovery kit with a new display. However, the two TBSs were combined into one, which is now the only option available in TouchGFX Designer. I can see that this happened in the same new release of the TBS as the software for the display update was improved. You can also see it in the changelog. This is of course a bit unfortunate in your current situation.

Do you want to use the previous implementation, or do you primarily need assurance that this will not happen again? The change was made solely to simplify the complex and confusing software implementation. Therefore, the orientation will not be changed again - it was just an unavoidable side effect. I can locate the latest published version of the AU1-specific TBS and provide it to you if you would like .. ?

Best regards,
Johan

6 replies

PaulK101Author
Associate II
October 13, 2025

Just wanted to add that the orientation of my old project matches this:

STM32F469I.png

PaulK101Author
Associate II
October 13, 2025

Here is another one that matches my previous project.  

STM32F469I 2.png

So something changed - the new project, I just created a new one and put one button w/text.  Flipped 180.

TDK
Super User
October 13, 2025

There's usually an LCD setting for screen rotation and mirroring. Screens typically have a shorter product lifecycle. It's possible a new screen was sourced instead of an old one. Just a guess. The board has undergone something like 10 revisions per the product page.

Default orientation per the user manual seems to be rotated vs what you show.

TDK_0-1760391577518.png

 

Discovery boards aren't meant to be used in final products.

"If you feel a post has answered your question, please click ""Accept as Solution""."
PaulK101Author
Associate II
October 15, 2025

It's literally the same board - why is it flipped 5 months later when I create a new project?  If screen orientation isn't something that is easily set in TouchGFX, how can I trust my production hardware won't do the same thing if I do an update 5 months later? 

ST Employee
October 14, 2025

Hello @PaulK101.

The display is natively portrait, and the direction of the scanline cannot be changed. Therefore, converting it to landscape orientation requires specific handling. If it is simply set up as landscape, tearing will occur.

Previously, the conversion was performed manually by splitting the display into four blocks. However, this implementation was complex and confusing. Starting from version 3.0.19 of the TBS, this process was simplified. The display is now set up as portrait, and the Rotate90 feature in TouchGFX is used to rotate it. However, Rotate90 rotates in the opposite direction compared to the previous manual implementation. As a result, the display appears rotated 180° compared to your old project. If you prefer the old implementation, you should use TBS version 3.0.18 or older.

Best regards,
Johan

PaulK101Author
Associate II
October 15, 2025

If I go back to an older version, it won't work on this board.  It is the -AU1 version and it looks like it is the latest rev.

One curious thing - the .IOC from my old project is called  STM32F469I-DISCO-REV-AU1.IOC.  When I create a new project now, the file is called STM32F469I-DISCO.IOC.

Was there a change in TouchGFX Designer or is this board missing from list when I create a new project?

469 list.png

 

LCE
Principal II
October 15, 2025

That's why you either:

- do not simply update stuff you didn't write yourself, always keep the working versions of external sources

- test changes / stuff before production

PaulK101Author
Associate II
October 15, 2025

That's the point, I DID write it using TouchGFX.  I didn't write the code to draw every little pixel on the screen because I used TouchGFX.  I have the original code I did write and it still compiles and works correctly with the original orientation.

And this is a new project using the original dev board.  Not sure what your contribution to this thread is?

JohanAstrupBest answer
ST Employee
October 15, 2025

Previously, two TBSs were available in TouchGFX Designer for the STM32F469I-DK. One of these was called STM32F469I-DISCO-REV-AU1 and covered the new revision of the discovery kit with a new display. However, the two TBSs were combined into one, which is now the only option available in TouchGFX Designer. I can see that this happened in the same new release of the TBS as the software for the display update was improved. You can also see it in the changelog. This is of course a bit unfortunate in your current situation.

Do you want to use the previous implementation, or do you primarily need assurance that this will not happen again? The change was made solely to simplify the complex and confusing software implementation. Therefore, the orientation will not be changed again - it was just an unavoidable side effect. I can locate the latest published version of the AU1-specific TBS and provide it to you if you would like .. ?

Best regards,
Johan

PaulK101Author
Associate II
October 15, 2025

Thank you, that's the answer I was looking for - there was a change.  I just wanted to make sure this wasn't some weird glitch/wrong software version/me losing my mind.

This is a new project and the orientation doesn't matter.  I just wanted some confirmation before I continue so I would not have to worry about it flipping back mid project.