Question
Pre flashed firmware in STM32U575ZI-NUCLEO-AZ2
Hi,
I want to get the access to the default pre flashed firmware image flashed while receiving STM32U575ZI-NUCLEO-AZ2 eval board. Can you share that whole firmware project along with the source code?
Also, whether the UI is built using TouchGFX? If yes, is it also possible to share the TouchGFX project as well for the default firmware on the eval board?
Thanks,
Mehul