[Problem] Unexpected error has happened
Unexpected error has happened
=======================================================================================
Sorry - something unexpected has happened which caused an error to occur in the Designer.
For more information, see the log file located at: C:\Users\sohae\AppData\Roaming\TouchGFX-4.25.0\TouchGFXDesigner.log
Please consider reporting this bug and steps to reproduce it at the TouchGFX Help Center so it can be fixed in a future version.
You can find the Help Center here: https://community.st.com/touchgfx
Error: Object reference not set to an instance of an object.
=======================================================================================

I installed torchgfx 4.25.0 today.
When I select 'Animated Image Example' from examples and click the create button,
I get the following error message.
How do I fix this?