Problem with CRC module on touchgfx in stm32h7 ?
Hello, I'm working with the STM32H7B3I-DK.
Info:
1- STM32H7B3I-DK (STM32H7B3LIH6QU)
2-STM32CUBEIDE rev: 1.6.1
3- TouchGfx rev: 4.16.1
I want to use the CRC module for data verification (16 bit).
Problem:
when I use the CRC default version everything works fine
hcrc.Instance = CRC;
hcrc.Init.DefaultPolynomialUse = DEFAULT_POLYNOMIAL_ENABLE;
hcrc.Init.DefaultInitValueUse = DEFAULT_INIT_VALUE_ENABLE;
hcrc.Init.InputDataInversionMode = CRC_INPUTDATA_INVERSION_NONE;
hcrc.Init.OutputDataInversionMode = CRC_OUTPUTDATA_INVERSION_DISABLE;
hcrc.InputDataFormat = CRC_INPUTDATA_FORMAT_BYTES;
if (HAL_CRC_Init(&hcrc) != HAL_OK)
{
Error_Handler();
}
But when I use this version of CRC to calculate my crc on my data, there is a problem with touchgfx (touchgfx_init)
hcrc.Init.DefaultPolynomialUse = DEFAULT_POLYNOMIAL_DISABLE;
hcrc.Init.GeneratingPolynomial = CRC_POLYNOMIAL_VALUE;
hcrc.Init.CRCLength = CRC_POLYLENGTH_16B;
hcrc.Init.DefaultInitValueUse = DEFAULT_INIT_VALUE_ENABLE;
hcrc.Init.InputDataInversionMode = CRC_INPUTDATA_INVERSION_NONE;
hcrc.Init.OutputDataInversionMode = CRC_OUTPUTDATA_INVERSION_DISABLE;
hcrc.InputDataFormat = CRC_INPUTDATA_FORMAT_BYTES;
if (HAL_CRC_Init(&hcrc) != HAL_OK)
{
Error_Handler();
}
Error :
in touchgfx_init function
FrontendHeap::getInstance()
touchgfx::Screen::draw()
"<signal handler called>() at 0xffffffe9"
HardFault_Handler
I do not understand why.
Is there a problem with touchgfx and CRC module?
Thanks in advanced to all your replies