Skip to main content
Visitor II
April 14, 2025
Question

Questions regarding invalidate() and draw()

  • April 14, 2025
  • 1 reply
  • 433 views

Hi!

We got an old TouchGFX (4.10) application where the screen freezes from time to time. Freeze means we no longer get tick events, whereas the other FreeRTOS tasks are still alive. *Most* times this happens after Button pressed events.

This raises understanding questions on our side:

  • I presume that calling invalidate() puts the drawable object in some kind of a queue, right?
    • What happens if invalidate() is called twice or more times on the same drawable object? Is the drawable queued twice or more times and is this drawable object drawn twice or more times?
  • What happens if a drawable object is
    - completely
    - partially
    hidden by an upper drawable object and invalidate() is called? (All drawables are set visible). Is the (partially) hidden drawable object drawn (completely) in both cases?
  • Is it possible to query an drawable object whether it has already been queued after a invalidate() call?
  • Lets pretend a Button changes its image on a Button pressed event. From our understanding there're two re-draw events:
    - Re-draw the old image when the button is released (triggered by TouchGFX framework).
    - Re-draw the new image as a result of the Button pressed event (triggered by us).
    Are these two events drawn in the same tick? Meaning in the same update phase?
  • Lets pretend a Button is within a Container and the Container is moved/slided/animated out of the Screen on a Button pressed event. We see here are two re-draw events as well:
    - Re-draw the old image when the button is released (triggered by TouchGFX framework).
    - Re-draw the container (incl. the Button) when starting to move/slide/animate the container out of the Screen (triggered by us).
    Are these two events drawn in the same tick? Meaning in the same update phase?
  • Is it possible that the invalidate() queue gets overcrowded?

Regarding the missing the tick events in our application: Are there any (known) user errors when using TouchGFX that prevents the TouchGFX framework from sending tick events? Or to ask the question the other way: That must have gone wrong that the TouchGFX framework stopped sending tick events?

Thank you for your help.

1 reply

GaetanGodart
Technical Moderator
May 5, 2025

Hello @hvv ,

 

4.10 is quite old now, I don't think I can help you much on your 4.10 freeze issue but I can answer your other questions.

 

Calling invalidate() on an area adds that area to the area that will be re-drawn, so if you call invalidate twice on the same area, it won't re-draw twice since this is the same area.

If you have 2 elements, element 1 is below and element 2 is above and partially hiding elemnt1, if you invalidate element 1, the area of element 1 will be invalidated including the part that is hidden, so if you change the color of element 2 but don't invalidate it, then you change the color of element 1 and invalidate element 1, then the visible part of element 1 will change color and the port of element 2 that is on top of element 1 will also change color.

If there are 2 re-draw events, only one re-draw will happen : the last one that happen right before the re-draw.

If 2 redraw such as one container and one button have to be re-draw, they will be re-drawn during the same tick if their invalidate happens at the same tick too.

 

Regards,