Resizing camera images
Hi everyone,
I have a screen project displaying a camera image using an STM32N6. I've validated and run several peripherals like DCMIPP and DMA2D. I'm currently displaying a 720x576 resolution image from DCMIPP on the screen via layer 2 using bitmap addressing.
My question is: Since I'm using internal RAM, Touchgfx uses one layer, and one layer is used for the camera. Because I'm not processing any bitmaps and need space, I've significantly reduced the size of the cmd_list area. After adding all this, I have about 300kB of free RAM left.
Now, what I need is to be able to see this camera image in full size on my 1024x600 px screen. However, I want to know if this enlargement is possible and if it requires a cmd_list, i.e., vector graphics.
Will I use vector graphics for this? Will GPU2D use the RAM allocated for layer 2 for this operation, or will it require an additional amount of RAM equal to the screen size?
Best Regards,
Onur