Riverdi STM32 Embedded 12.1" Display only displaying a blackscreen
Hello, how is everyone doing ?
I am making this post because I just received a Riverdi STM32 Embedded display for my last ever studying project, as I will use it to replace 7-seg, buttons and keybord. I made a simple connection for the power supply (I soldered two wires on the connector, to avoid cutting the given cable, as I want to use it later in the final version of my project. My problem is that when I turn on the power, the screen switches on but only displays a black screen at maximum brightness. I tried reseting the device with the back button, and also created a simple TouchGFX project to display a png image and the memory flash of the microcontroller with ST-Link v2 works fine but once the flash is done, the screen goes back to the very bright black screen state.
I have made some research but have not found anything interesting, so I make this post hoping that someone already had this issue or has a solution. In the meantime I have also contacted Riverdi, but I want an answer as soon as possible, so I ask your community !
Thanks in advance.