Running 10.1" LVDS display on (STM32747I-Disco) discovery board
I wonder if there are any discovery or evaluation boards that directly support connection to a 10.1" screen, and please do respond with something other than Riverdi. It would be nice if one could develop its own hardware without being overly dependent on third parties such as Riverdi. Has anyone managed to use the STM32747I-DISCO board (or any other board for that matter) with a bare 10.1" screen that has a 40-pin LVDS connector? So far I have only seen examples using the DISCO board with smaller screens. The 60-pin connector on the DISC board seems to carry a number of differential clock and data signals, so this looks like LVDS. Is it just a question of making a mechanical adapter from one connector to another?