Same TouchGFX project for multiple CubeMX files in the same CubeIDE project
Hello,
To elaborate on what I mean and wondering about with the subject using an example:
I am using one CubeIDE project to develop an application for two different hardware boards using the same MCU. Each of these boards have a CubeMX file associated with it since the pinout of the boards differ somewhat. But most of the functionality is the same between the boards, and they share the code on an application layer. I use ifdefs and build configurations to build the desired application.
Right now, I have a double set of all TouchGFX related files, one in the CubeMX folder for HW1 and one for HW2, which are a complete copy of the other. I instead want to move this code to the application layer level since the code is the same, and changes to the GUI would be implemented to both hardware applications with one change.
How would I go by doing this? Since the code generation is coupled tightly with CubeMX, can it even, somewhat easily, be done in a reliable way?
I guess this somewhat also extends to how one would maintain and update a GUI which is used in multiple projects in an easy way. In my head, having the GUI as a module that would be loaded into the desired application would be an option, but I have not found any source about this being done. Does anyone have any input or inspiration here?
Regards,
Pontus