STMH7S7 CUBEIDE,Post Generate Target failed。
I made a test project for h7s7 using cubeIDE,the structure generated is below:

Then I opened touchgfx designer and import a blank UI, when I tried to build the project, a error came out:
Generate Code
Generate
Wrote generated/gui_generated/include/gui_generated/screen1_screen/Screen1ViewBase.hpp
Wrote generated/gui_generated/src/screen1_screen/Screen1ViewBase.cpp
Done
Generate Assets
make -f simulator/gcc/Makefile assets -j8
Reading ./application.config
Reading ./target.config
Done
Post Generate
touchgfx update_project --project-file=simulator/msvs/Application.vcxproj
Done
Post Generate Target
touchgfx update_project
Unable to locate D:/STM32CubeIDE/workspace_1.7.0/7s7Test/.cproject
Failed
Failed
The .cproject is actually located in D:/STM32CubeIDE/workspace_1.7.0/7s7Test/Appli/.cproject
but touchgfx designer goes to wrong folder.
Anyone who can help?