Skip to main content
Associate
October 1, 2025
Solved

Stride Value is Readonly after Update to TouchGFX 4.26

  • October 1, 2025
  • 2 replies
  • 322 views

After updating TouchGFX from 4.24.1 to 4.26.0, the Stride setting in "X-CUBE-TOUCHGFX"->"TouchGFX Generator" is readonly (grayed out). I need to set it to the value 832.

gerthmar_0-1759306845114.png

 

The generated code uses the value 800, even if I modify the value in the project.ioc file manually.

When I change the Stride value in TouchGFXHAL.cpp and in TouchGFXGeneratedHAL.cpp (at call of setFrameBufferSize()) manually, the display works perfectly.

I am using:

  • STM32F769BIT uC
  • MxCube 6.15.0
  • STM32Cube FW_F7 V1.17.4

 

Any advise is very welcome. Thank you!

 

Best answer by STackPointer64

Hello @gerthmar,

After checking, it appears the configuration method was updated. The stride value can still be modified through the LTDC panel inside the Layer Settings tab, under Frame Buffer Configuration, by changing Layer 0 - Color Frame Buffer Line Length (Image Width). The previous method in TouchGFX 4.25.0 was incorrect, as it could cause issues and user frustration due to potential misconfigurations. The new approach is an improvement and more accurate.

Best regards,

2 replies

Technical Moderator
October 1, 2025

Hello @gerthmar, and welcome to ST Community!

I have escalated the issue to the relevant team for resolution. It is being tracked internally under ticket number 218772.

Best regards,

To improve visibility of answered topics, please click 'Accept as Solution' on the reply that resolved your issue or answered your question.
STackPointer64Best answer
Technical Moderator
October 3, 2025

Hello @gerthmar,

After checking, it appears the configuration method was updated. The stride value can still be modified through the LTDC panel inside the Layer Settings tab, under Frame Buffer Configuration, by changing Layer 0 - Color Frame Buffer Line Length (Image Width). The previous method in TouchGFX 4.25.0 was incorrect, as it could cause issues and user frustration due to potential misconfigurations. The new approach is an improvement and more accurate.

Best regards,

To improve visibility of answered topics, please click 'Accept as Solution' on the reply that resolved your issue or answered your question.
gerthmarAuthor
Associate
October 3, 2025

Thank you @STackPointer64 . That solves the problem!

Best regards!