Skip to main content
afergan
Associate II
February 14, 2023
Question

TouchGFX 4.21.1 Causing Distortion on Moving Images

  • February 14, 2023
  • 3 replies
  • 1327 views

I have custom clock widget in my project and its working fine on version 4.20 but when i upgraded it to 4.21.0 or 4.21.1 causing distortion on clock hands.

When I investigate the issue I saw that SCB_CleanInvalidateDCache() function removed from TouchGFXGeneratedHAL::flushFrameBuffer function. Here is the old function 4.20 has;

void TouchGFXGeneratedHAL::flushFrameBuffer(const touchgfx::Rect& rect)

{

    HAL::flushFrameBuffer(rect);

    // If the framebuffer is placed in Write Through cached memory (e.g. SRAM) then

    // the DCache must be flushed prior to DMA2D accessing it. That's done

    // using the function SCB_CleanInvalidateDCache(). Remember to enable "CPU Cache" in the

    // "System Core" settings for "Cortex M7" in CubeMX in order for this function call to work.

    if (SCB->CCR & SCB_CCR_DC_Msk)

    {

        SCB_CleanInvalidateDCache();

    }

}

When I add this manually its working fine. I didnt understand why they removed this part of code in new version.

There is 2 more functions doing same cache clean;

void TouchGFXGeneratedHAL::InvalidateCache()

{

    // If the framebuffer is placed in Write Through cached memory (e.g. SRAM) then

    // the DCache must be flushed prior to DMA2D accessing it. That's done

    // using the function SCB_CleanInvalidateDCache(). Remember to enable "CPU Cache" in the

    // "System Core" settings for "Cortex M7" in CubeMX in order for this function call to work.

    if (SCB->CCR & SCB_CCR_DC_Msk)

    {

        SCB_CleanInvalidateDCache();

    }

}

void TouchGFXGeneratedHAL::FlushCache()

{

    // If the framebuffer is placed in Write Through cached memory (e.g. SRAM) then

    // the DCache must be flushed prior to DMA2D accessing it. That's done

    // using the function SCB_CleanInvalidateDCache(). Remember to enable "CPU Cache" in the

    // "System Core" settings for "Cortex M7" in CubeMX in order for this function call to work.

    if (SCB->CCR & SCB_CCR_DC_Msk)

    {

        SCB_CleanInvalidateDCache();

    }

}

But I can't see any call for this functions. Is this a migration issue or something wrong with my project?

Thanks.

This topic has been closed for replies.

3 replies

Osman SOYKURT
Technical Moderator
February 15, 2023

Hello afergan,

Which TBS is your project based on ? I'll try to investigate on this issue..

/Osman

Osman SOYKURTST Software Developer | TouchGFX
afergan
aferganAuthor
Associate II
February 15, 2023

Hi @Osman SOYKURT​ ,

 

I'm using custom board not ready to use ones. I have STM32H743VIT6 on this board and using LTDC + DMA2D for filling the screen. And ICache and DCache are enabled in my project.

 

On TouchGFX 4.20 TouchGFXGeneratedHAL::flushFrameBuffer have SCB_CleanInvalidateDCache(); call inside by default. But after updating 4.21 this function call removed. I can still add it manually and its working but I couldn't understand why this line was removed.

Lead II
March 12, 2024

Indeed. I have the same question. In the documentation of TouchGFX it says these methods are called by the framework, but they aren't.

https://support.touchgfx.com/docs/development/board-bring-up/how-to/02-cpu-running

"When the state transit from HARDWARE to SOFTWARE it will call the virtual method void touchgfx::HAL::InvalidateCache() and when the state transitions from SOFTWARE to HARDWARE it will call the virtual method void touchgfx::HAL::FlushCache(). The functionality of these two functions is left for the user to implement in the derived HAL class."
Maybe I don't fully understand what they mean with the transition. It uses either sw or hw rendering as far as I know. Now I always clear the cache in flushFrameBuffer, but maybe that is not needed?

"Kudo posts if you have the same problem and kudo replies if the solution works.Click ""Accept as Solution"" if a reply solved your problem. If no solution was posted please answer with your own."
Yoann KLEIN
ST Employee
February 15, 2023

Hello @afergan​,

Please take a look at this article, it explains how the switch mechanism between HW/SW rendering works.

/Yoann