Skip to main content
Associate II
August 6, 2024
Solved

Touchgfx and HAL_GPIO_WritePin in simulator

  • August 6, 2024
  • 5 replies
  • 2069 views
This piece of code works if I transfer it to my board, but if I use the simulator in TouchGFX, I get an error: gui/src/model/Model.cpp:7:10: fatal error: main.h: No such file or directory #include "main.h".
 
Screen1View.cpp
#include "stm32f7xx_hal.h"
 
// LED Toggle function
void Screen1View::ToggleLED()
{
 if (toggleButton1.getState()) HAL_GPIO_WritePin(GPIOA, GPIO_PIN_0, GPIO_PIN_SET);
 else HAL_GPIO_WritePin(GPIOA, GPIO_PIN_0, GPIO_PIN_RESET);
}
 
I am using TouchGFX 4.24
BR 
Best answer by unsigned_char_array

@LouisB wrote:

 

#ifdef SIMULATOR

 // Your simulator specific user code here

 #include "gui/common/myInclude.hpp"

#else
 // Your hardware specific user code here

 extern "C"

 {

 #include "stm32f7xx_hal.h"

 }

#endif
 

 

 


extern C is not needed as stm32f7xx_hal.h already has this inside the header file. As far as I know all ST header files are like this.

 

This would work:

 

#ifndef SIMULATOR
#include "stm32f7xx_hal.h"
#endif

// LED Toggle function
void Screen1View::ToggleLED()
{
	if (toggleButton1.getState())
	{ 
		#ifndef SIMULATOR
		HAL_GPIO_WritePin(GPIOA, GPIO_PIN_0, GPIO_PIN_SET);
		#else
		//simulate an LED on the screen, for example
		#endif
	}
	else
	{
		#ifndef SIMULATOR
		HAL_GPIO_WritePin(GPIOA, GPIO_PIN_0, GPIO_PIN_RESET);
		#else
		//simulate an LED on the screen, for example
		#endif
	}
}

 

 

5 replies

amigafanAuthor
Associate II
August 6, 2024

Ups, the error is:gui/src/model/Model.cpp:7:10: fatal error: stm32f7xx_hal.h: No such file or directory #include "stm32f7xx_hal.h". Sorry

ST Employee
August 6, 2024

Hello @amigafan ,


How did you include the file in your project ? The board and the simulator are built differently.

 

Best regards,
Louis B.

amigafanAuthor
Associate II
August 6, 2024

?? I wrote #include "stm32f7xx_hal.h" in Screen1View.cpp.

Br

ST Employee
August 6, 2024

I meant in which folder did you put the file ?

amigafanAuthor
Associate II
August 6, 2024

It is in STM32CubeIDE, I dit no add a file to any folder.

ST Employee
August 9, 2024

Hello @amigafan,

The issue is the file itself, it's an hardware specific file that will only work on target.

 

#ifdef SIMULATOR

 // Your simulator specific user code here

 #include "gui/common/myInclude.hpp"

#else
 // Your hardware specific user code here

 extern "C"

 {

 #include "stm32f7xx_hal.h"

 }

#endif
 

 

I hope it helps,
Best regards

Lead II
August 9, 2024

@LouisB wrote:

 

#ifdef SIMULATOR

 // Your simulator specific user code here

 #include "gui/common/myInclude.hpp"

#else
 // Your hardware specific user code here

 extern "C"

 {

 #include "stm32f7xx_hal.h"

 }

#endif
 

 

 


extern C is not needed as stm32f7xx_hal.h already has this inside the header file. As far as I know all ST header files are like this.

 

This would work:

 

#ifndef SIMULATOR
#include "stm32f7xx_hal.h"
#endif

// LED Toggle function
void Screen1View::ToggleLED()
{
	if (toggleButton1.getState())
	{ 
		#ifndef SIMULATOR
		HAL_GPIO_WritePin(GPIOA, GPIO_PIN_0, GPIO_PIN_SET);
		#else
		//simulate an LED on the screen, for example
		#endif
	}
	else
	{
		#ifndef SIMULATOR
		HAL_GPIO_WritePin(GPIOA, GPIO_PIN_0, GPIO_PIN_RESET);
		#else
		//simulate an LED on the screen, for example
		#endif
	}
}

 

 

"Kudo posts if you have the same problem and kudo replies if the solution works.Click ""Accept as Solution"" if a reply solved your problem. If no solution was posted please answer with your own."