Associate II
January 4, 2025
Question
touchgfx breaks ethernet connection
- January 4, 2025
- 1 reply
- 491 views
I customized a board with stm32h743iit6 for HMI application, the main hardware features available on the board are RMII ethernet, 32bit SDRAM and LTDC RGB565 interface. Below is the board picture.

A test MDK keil project is generated by cubemx to test ethernet communication, freertos and lwip are enabled.
Packet loss ratio is zero even for a very long time test, and tcp echo application works fine.

But packet loss ratio rises to about 0.1% when touchgfx added to the project. if interacting with touchgfx screen, ethernet connection will break immediately,while touchgfx still works correctly.
I have tried to improve priority and increase stack size of lwip thread, still can't solve it.
what did I miss?
here is the cubemx config file.