TouchGFX buttons will not trigger in lower area of STM32F469I-Disco display
Dear
I'am protoyping a GUI on a STM32F469I-Disco board and encounter the "feature" that buttons in the lower area of the canvas will not trigger when touched (e.g. the red circled "Auto"). Strangely when moving these buttons (e.g. "00.000V") to the upper area without changing anything else the suddenly work????
Of course my first suspect was the FT6xxx touch controller chip, so I debugged into the STM32TouchController::sampleTouch(int32_t& x, int32_t& y) function. I confirmed that the touch controller worked as designed delivering proper coordinates on every touch (origin in the upper right corner, x increasing down, y increasing to the left)
As of now I've no clue where to look, help appreciated!
Thx MT
P.S.: The canvas has been configured in landscape orientation in TouchGFX designer