TouchGfx generated project name
Here is what I see as ST's idea of a TouchGfx workflow.
Create a GUI project, import that project into an IDE, which in my case would be STM32CubeIDE.
Click on the .project file to import into the IDE with the same name as the board. (Disregard and project name provided during the TouchGfx project creation.)
Experiment with the project, jump back and forth between TouchGfx and the IDE.
Throw the project away and you're on your own as to how to create a standalone GU project with STM32CubeIDE.
Nice, for seeing examples but essentially useless for creating a basis for a real project.
A real workflow would allow you to generate a TouchGfx project with an .ioc and a .project reflecting a name you want to use rather than the board name. I don't want to use CubeMX to manually adjust many pins and parameters in order to have the board be functional as the base for a GUI.
It would provide a way of importing into the IDE, that allowed for the file structure created within TouchGfx to be totally integrated into the local workspace in such a way that you could still jump back and forth between the IDE and TouchGFX.
I've seen this issue touched on over and over and haven't seen a viable solution. Modifying file names and .project file contents to fit within the desired IDE structure, works for compilation, but doesn't allow you to go back to TouchGFX to modify the GUI, without once again modify filenames and .project files.
I haven't seen one solution that gets me an STM32CubeIDE solution with the names I want that still allows the use of both tools without messing with names and content.
Just modifying TouchGfx Designer to create projects and .ioc files with the names provided as the project name would go a long way toward a viable development workflow. I would be interested to know why the designers of TouchGFX decided to name every project and .ioc file the same name as the board. This prevents a user's ability to import two GFX projects into the same workspace!
I don't believe you can provide me with a method to accomplish what I want within the existing software infrastructure. Consider this a suggestion for an immense improvement.