Skip to main content
PFlor.2
Senior II
November 25, 2024
Solved

TouchGFX not running on STM32H563 with SPI LCD interface and FreeRTOS

  • November 25, 2024
  • 1 reply
  • 750 views

I’m not sure why TouchGFX doesn’t seem to be running in a new H563 project when I’ve done this on the H743 on a previous project.  The last project did use LTDC instead of SPI for the display interface so maybe that has something to do with it.  I have confirmed the SPI drivers for the LCD by painting an entire screen from a buffer of color pixels.

Right now I just have a single simple screen created in TouchGFX with internal memory set for assets.

PFlor2_0-1732574243284.png

PFlor2_1-1732574274237.png

I setup the ToughGfxTask as described in the TouchGFX documentation for FreeRTOS…

Real Time Operating System | TouchGFX Documentation

PFlor2_2-1732574309529.png

PFlor2_3-1732574337286.png

I then setup the SPI display interface to TouchGFX as described in documentation…

FMC and SPI Display Interface | TouchGFX Documentation

PFlor2_4-1732574377456.png

PFlor2_5-1732574410949.png

Where can I set a breakpoint to see if the TouchGFXTask is running?  I never reach a breakpoint in this flushFrameBuffer().

I see the TouchGFXTask startup function TouchGFX_Task() does execute…

PFlor2_6-1732574453519.png

Since I’m using the internal flash for TouchGFX there’s nothing need in the linker script STM32H563RGTX_FLASH.ld yet right?  My understanding is I just need to map external flash once I have that setup, just using internal to get things running initially before getting the QuadSPI for the external flash implemented.

 

 

 

 

Best answer by PFlor.2

All examples I had seen for SPI display interface to TouchGFX used a partial frame buffer.  When using single/double framebuffer configuration it is still necessary to use a task or timer to trigger a signalVSync() function for TouchGFX to send screen data to the application/LCD driver.

PFlor2_0-1733498947922.png

In my particular case, I created a task to call the function above every 100ms.  Based on my framebuffer size and SPI baudrate (15MBits/s) I was able to take it down to every 82ms (screen size 320x240):

320 x 240 x 2 x 8 = 1228800 / 15000000MBits/s = 0.08192s = 81.92ms

Also, for my SPI driver the loop to write framebuffer data 1 line at a time did not work well and was better suited to send entire buffer to driver at once....

PFlor2_1-1733499381532.png

 

1 reply

PFlor.2
PFlor.2AuthorBest answer
Senior II
December 6, 2024

All examples I had seen for SPI display interface to TouchGFX used a partial frame buffer.  When using single/double framebuffer configuration it is still necessary to use a task or timer to trigger a signalVSync() function for TouchGFX to send screen data to the application/LCD driver.

PFlor2_0-1733498947922.png

In my particular case, I created a task to call the function above every 100ms.  Based on my framebuffer size and SPI baudrate (15MBits/s) I was able to take it down to every 82ms (screen size 320x240):

320 x 240 x 2 x 8 = 1228800 / 15000000MBits/s = 0.08192s = 81.92ms

Also, for my SPI driver the loop to write framebuffer data 1 line at a time did not work well and was better suited to send entire buffer to driver at once....

PFlor2_1-1733499381532.png