TouchGFX project: FreeRTOS or ThreadX available, but not AzureRTOS ?
Hello,
I successfully improved the TouchGFX based Clock Example demo app to use RTC chip (and LSE crystal clock) of the N6570 MCU. Because the STM32N6570-DK board does not provide backup battery the RTC loses the current date/time during every power off. One solution would be to sync the RTC chip with an SNTP server via Internet. I successfully solved this with STM32H7474I-DISCO board with LwIP and SNTP client, but the STM32N6570-DK board does not support LwIP.
I found an example for the STM32N6570-NUCLEO-144 board which is probably similar (or close) to STM32N6570-DK board. The problem is that the found Nx_SNTP_Client application uses NetXDuo and AzureRTOS while my project runs under FreeRTOS op system.
How can I solve this? When create a new TouchGFX project I can choose between FreeRTOS or ThreadX op systems only. I can't use AzoreRTOS...
Can anybody help?
Thanks,
Louis