Skip to main content
Associate II
June 9, 2025
Question

TouchGFX Source Generation Failing After Disabling DSI for RGB-888 (H757 Eval Kit)

  • June 9, 2025
  • 6 replies
  • 945 views

We are facing a technical issue creating a TouchGFX project. We suspect it is an inherent issue with ST’s toolchain —STM32CubeMX and TouchGFX—when used with the official STM32H757 Eval Kit.

Issue at Quick Glance:
1. Enabling LTDC in STM32CubeMX automatically enables DSI, even when we intend to use only RGB888 via CN20 (as in our custom display board with 10.1inch Winstar WF101JTYAHLNB0#).
2. This causes build failures and prevents TouchGFX Designer from generating any GUI code, despite the project being valid and configured as per ST training examples.
3. We’ve attempted all known workarounds, including patching headers and ensuring paths/configs are correct—yet the issue persists.


We kindly request:
1. Resolution on how to disable DSI cleanly while keeping CubeMX and TouchGFX code generation functional.
2. Clarification on internal tool dependencies between LTDC and DSI, and how to bypass them for RGB-only use cases.
3. A reference TouchGFX project using only RGB+LTDC (via CN20) for STM32H757 Eval Kit.

This is a time-sensitive issue. We’re happy to provide our .ioc, test project zip if needed for detailed analysis and support.
We look forward to your expert guidance.

6 replies

GaetanGodart
Technical Moderator
June 11, 2025

Hello  @vijay29489 ,

 

On their website, on the product page, Winstar advertise its display with TouchGFX, perhaps you should reach out to them to see how they intend you to use the display? Maybe there is good information on their documentation too?

1)
The display you want to use in a TFT LCD display, so LTDC is what you need. Why do you want to only use DSI and not LTDC?

 

2)
You say that it prevents code generation even if the project is valid, but it is probably because the project is not valid that TouchGFX (and STM32CubeMX?) refuse to generate code.

 

1)
You can disable DSI through STM32CubeMX and generate code through STM32CubeMX but then the TouchGFX project won't work anymore as there won't be a way to control the screen.
Therefore, what you want to do is to disable whatever screen control you have enabled and enable another screen control. But in your case, you need LTDC for the TFT CLD Winstar display I think.

 

2)
DSI is required for MIPI DSI displays, in that case, LTDC takes care of pixel data and synchronization and DSI Host act as a bridge between DSI and LTDC.

 

Can you tell me what steps you took to try and make your STM32H757 eval board work with the Winstar display?

Sharing your ioc file could help aswell.

 

Regards,

Associate II
June 11, 2025

Hi Gaetan Godart,

Thanks again for your reply and for continuing to support this.

Just to clarify — we are not using DSI in our setup. The display we’re working with (Winstar WF101JTYAHLNB0#) is an RGB888 TFT panel connected via CN20 on the STM32H757 Eval Kit. We are using LTDC only.

The issue we’re facing is that when we enable the LTDC peripheral, the DSIHOST is automatically selected for the CM7 core. This causes the DSI to be defined at line 30 instm32h7xx_hal_ltdc_ex.h, which in turn includes stm32h7xx_hal_dsi.h at line 32. As a result, our code fails to compile. On top of that, TouchGFX Designer refuses to generate GUI code because of this.

We’ve tried several workarounds — disabling DSI in CubeMX, manually removing DSI config from the generated code, patching the HAL files — but they either get overwritten or cause other toolchain issues.

As requested, I’ve attached our 'Test_RGB.ioc' file for your reference. The project is configured for LTDC + RGB888 only (no DSI), and you can recreate it in STM32CubeMX directly using this file.

Could you please help us understand how to cleanly use LTDC without DSI in this case? Is this a known issue with CubeMX or TouchGFX integration? And is there any working example project for STM32H757 Eval Kit using just LTDC and RGB?

Appreciate your help on this — we’re on a tight timeline and would really value your guidance to get past this blocker.

Best regards,
Vijaykumar Vishwakarma
Senior Manager, Technical Architect- Firmware

Syrma Johari Medtech Ltd
Attachment: Test_RGB.ioc

GaetanGodart
Technical Moderator
June 12, 2025

Hello @vijay29489 ,

 

The ioc file you shared is for STM32H747, not STM32H757 :

GaetanGodart_0-1749730137870.png

 

When enabling LTDC, you have to select the pixel format. You can choose "RGB888" or "RGB888 for DSI".

When switching from one to another you see that your LTDC configuration changes. So just stay with "RGB888" (not DSI) even if it keep DSI enabled.

The ioc you shared also have other issues such as wrong start and stop value or double layer even if TouchGFX only support single layer.

 

It is not recommended to change the generated code as it will be re-generated if you change the STM32CubeMX setup.

By not changing the code you should be able to build and flash (perhaps with a wrong behavior but it should build and flash).

 

Can you explain to me why you want to disable DSI? Is it because you want to use the pins used by DSI?

Also, can you explain to me how the Winstar display must be controlled? I see on the product page "UART" which is unusual to me.

 

Regards,

Associate II
June 13, 2025

Hello Gaetan,

1. You're correct—the .ioc file is for the STM32H747. I initially worked with the STM32H757 and encountered issues, so I generated sample code using TouchGFX Designer, which defaults to STM32H747. Since both controllers (and their eval kits) are fundamentally the same, the generated code runs correctly on the STM32H757 eval kit.

2. I did configure LTDC in STM32CubeMX with 1 layer and RGB888 pixel format, and I haven’t modified the generated code. If the shared .ioc file appears otherwise, I apologize—it was not intentional, and I’ve followed the correct setup as you pointed out.

3. I plan to disable DSI because we’re using a 10.1" touch display that requires LVDS data format. Larger displays typically use LVDS, so we’ll use the parallel RGB888 output from our controller with an LVDS converter (DS90C385A) and then interface with the display.

If possible, requesting you, could you please update the shared .ioc file and send it back to me? If I’ve made any mistakes in generating the project, I’ll make sure to correct them.

Best regards,
Vijay

GaetanGodart
Technical Moderator
June 13, 2025

Hello @vijay29489 ,

 

It seems that DSI is defined but there must be a confusion in the naming because it DSI being defined doesn't mean that DSI is enabled but only that the address is known.
Which means that it tries to include the DSI header which you don't have if you disable DSI in STM32CubeMX.

So a fix is to add the DSI header (please find it attached) to your Core => Inc folder :

GaetanGodart_0-1749814728461.png

We will investigate internally to fix this issue, thank your for bringing it up.

 

Regards,

Associate II
June 18, 2025

Hi Gaetan,

Thank you very much for promptly sharing the dsi.h file and the corresponding fix — that part is now working well.

However, we’re still facing an issue with the TouchGFX code compilation. After opening the .touchgfx file in TouchGFX Designer and making any screen design changes, the generated code does appear correctly in the STM32CubeIDE project. But when we try to compile the project, it throws numerous errors related to TouchGFX.

To help us move forward more efficiently, could you please share a sample project if available — ideally with a simple screen setup that’s compatible with our display configuration? This would be extremely helpful for reference and validation.

We’re hopeful this can be resolved quickly so we can get the display up and running. If you need specific error logs or screenshots to assist with troubleshooting, we’d be happy to provide them.


Best regards,
Vijay

GaetanGodart
Technical Moderator
June 23, 2025

Hello @vijay29489 ,

 

I was sick last week :\

I am afraid that we don't have a project with a similar screen and setup.

Could you please indeed share screenshot and logs of the errors you encounter.

 

Is it the first time you try to setup a MCU + display to run TouchGFX?

 

Regards,

Associate II
June 25, 2025

Hi Gaetan,

Apologies for the late reply as I was busy with other important activities.

We had full success with TouchGFX and STM32H757 eval kit using onboard display interfaced over DSI, but are now facing issues after switching to our custom LVDS setup. I’ve attached the build_logs_with_error.txt showing the compilation errors we are getting.

I’m reviewing 'AN4861 - Overview of LTDC controller and STM32 MCUs graphical portfolio' document to understand and rebuild the project and avoid further issues. Any support from your side would be appreciated.

Best regards,
Vijay

GaetanGodart
Technical Moderator
June 26, 2025

Hello @vijay29489 ,

 

How did you create this new project?

It seem it is only "no such file or directory" issues that are caused because the compiler doesn't know where to look for files.

Could you try to add (or verify that they are added) the paths where you have the various files not found?

 

Regards,