Skip to main content
Associate
April 29, 2024
Question

TouchGFX Usage Issues

  • April 29, 2024
  • 3 replies
  • 1842 views

"I've tried reinstalling, but I'm still encountering the following errors:

  • TouchGFX 4.23.2: Unable to download Demo project and Generate Code.
  • TouchGFX 4.20.0: Can download Demo project but unable to Generate Code.
  • TouchGFX 4.16.0: Able to Generate Code but encountering TCP/IP errors."
This topic has been closed for replies.

3 replies

ST Employee
April 30, 2024

Hello @mimiRJay ,

First, Welcome to the TouchGFX forum.

Can you tell me, which version of windows you are using ?

Regards,

mimiRJayAuthor
Associate
April 30, 2024

Hello @LouisB

windows  10

ST Employee
May 3, 2024

Hi @mimiRJay,


In the 4.16, by TCP/IP issue, you are talking of not being able to download Demos ? That's a known issue that is not related to Touch GFX directly.

In the 4.20 what's the generator error ? And in 4.23 can you check your proxy and also retry it ?

 

Regards,

mimiRJayAuthor
Associate
May 12, 2024

Hello @LouisB
When using the 'Generate Code' feature, an error occurred showing 'Generate Code Failed' (TouchGFX 4.20.0).
When using Generate Code functionality, encountering an error related to 'SSL/TLS secure channel' (TouchGFX 4.16.0).
When attempting to download certain examples, I'm unable to download them.(TouchGFX 4.23.2)

displays

~~~

Sorry - something unexpected has happened which caused an error to occur in the Designer.

For more information, see the log file located at: C:\Users\User\AppData\Roaming\TouchGFX-4.23.2\TouchGFXDesigner.log

Please consider reporting this bug and steps to reproduce it at the TouchGFX Help Center so it can be fixed in a future version.
You can find the Help Center here: https://community.st.com/touchgfx

Error: Object reference not set to an instance of an object.
~~~

 

MM..1
Chief III
May 12, 2024

Known Issues | TouchGFX Documentation start with visual C redist