Update a text area with a string and sting has \n newline char
I am trying to update a text area called textTestArea with a string and I want to be able to format the string with a newline character. Ex "I went to the store \n to buy food"
I created a texts called genericText that uses a default font that has wildcard range 0x00-0xFF , I also tried having range 0x20-0x7e and wildcard character 0x0A (/n)
here is the text and typography:


Here is the screen with text area:


in baseview.cpp it creates:
textTestArea.setPosition(397, 26, 237, 55);
textTestArea.setColor(touchgfx::Color::getColorFromRGB(0, 0, 0));
textTestArea.setLinespacing(0);
Unicode::snprintf(textTestAreaBuffer, TEXTTESTAREA_SIZE, "%s", touchgfx::TypedText(T_GENERICTEXT).getText());
textTestArea.setWildcard(textTestAreaBuffer);
textTestArea.setTypedText(touchgfx::TypedText(T___SINGLEUSE_E1ZC));
add(textTestArea);So now in my view.cpp:
static const uint16_t TEXTBUFFER_SIZE = 64;
Unicode::UnicodeChar textBuffer[TEXTBUFFER_SIZE];
Unicode::snprintf(textBuffer, TEXTBUFFER_SIZE, "I went to store \n to but food");
textTestArea.setTypedText(TypedText(T___SINGLEUSE_81C4)); // Must match your Texts View ID
textTestArea.setWildcard(textBuffer);
textTestArea.setWideTextAction(WIDE_TEXT_WORDWRAP);
textTestArea.resizeToCurrentText();
textTestArea.invalidate();I get "test" Not I went to the store....
I have tried 100 iterations. I have gotten it to print "I went to the store \n to buy food", but can not get it to acknowledge the \n character.
How is this implemented correctly?