X-CUBE-TOUCHGFX 4.23.2 is out!
TouchGFX 4.23.2 is now out.
Please follow this link to download it.
4.23.2 Release details:
Release date: March 14th, 2024
Bugfixes in TouchGFX Designer:
- Fixed a bug where TouchGFX Designer would not close properly
Bugfixes in TouchGFX Core:
- Fixed issue were accessing cached bitmap data could result in unaligned
memory accesses.
- Fixed issue were accessing cached bitmap data could result in unaligned
4.23.1 Release details:
Release date: January 22nd, 2024
Bugfixes in TouchGFX Designer:
- Fixed TextArea lineheight in canvas not matching with rendered lineheight.
- Fixed 'tgfx.exe generate' creating new 'touchgfx_backup' everytime it is executed.
- Fixed opening properties for 'Grid Lines' and 'Labels' on graph widgets enabling and disabling them.
- Fixed importing Custom Widgets with fonts causing issues.
New TouchGFX Core Features:
- Added methods SwipeContainer::goNextPage() and SwipeContainer::goPreviousPage() to change page with an animation.
Bugfixes in TouchGFX Core:
- Fixed issue where kerning data was sometimes missing for vector fonts.
- Fixed issue where CacheableContainer could draw outside the invalidated area.
- Drawing vector fonts on STM32U599/5A9 using GPU2D (NeoChrom) would result in poor anti-aliasing.
- Fixed Keil library nemagfx_core_release.lib to use lcd class "LCDGPU2D_AXI" instead of "LCDGPU2D" for cortex M7 and M55.
- New TouchGFX Generator Features:
- Support for TrustZone applications (STM32L5/STM32U5).
- Bugfixes in TouchGFX Generator:
- Having Video Decoding enabled on ThreadX applications would result in compilation errors when using MDKARM.
Note : TouchGFX Designer 4.23.2 MUST be used with STM32CubeMX 6.10.0 or above (link to download STM32CubeMX).
Attention : If X-CUBE-TOUCHGFX 4.23.2 is not available in STM32CubeMX software yet, please navigate to "Help > Manage embedded software packages > STMicroelectronics > X-CUBE-TOUCHGFX". Then click on "From Local ..." and navigate to the x-cube-touchgfx-4-23-2.zip file to install the new pack inside STM32CubeMX.
Please also check our Known Issues article.
Enjoy this new version ! :)