X-CUBE-TOUCHGFX 4.26.1 is out!
TouchGFX 4.26.1 is now out.
Please follow this link to download it.
This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.
Please visit our dedicated website for STM32H5 graphics to know more about high performance graphics on our most powerful Cortex-M33 MCU.
Release details:
- Release date: March 2nd, 2026
- New TouchGFX Designer Features
- Allow selecting a CMakeLists.txt file as the project file without requiring a STM32CubeMX .ioc file.
- Allow selecting a CMakeLists.txt file as the project file without requiring a STM32CubeMX .ioc file.
- Bugfixes in TouchGFX Designer
- Fix caching issue when changing text configurations and re-generating code.
- Fix outdated timestamp on files when importing a GUI.
- Fix faulty code generation when a Shape widget has two identical end points.
- Fix faulty code generation when a Shape widget uses an "interaction ended" callback.
- New TouchGFX Generator Features
- Support for STM32H5F5/E5 and STM32H5F4/E4 series with the new Chrom-Art 2 hardware accelerator.
- Bugfixes in TouchGFX Generator
- Fixed an issue where YCbCr video buffer sizes were generated incorrectly for some framebuffer width values.
- Fixed an issue where the task memory pool used by ThreadX was not aligned correctly.
- New TouchGFX Core Features
- Added Chrom-Art 2 support.
- Added Chrom-Art 2 support.
- Bugfixes in TouchGFX Core
- Fixed an issue where the noise function for 16-bit linear gradient painters compiled to incorrect instructions on some platforms.
- Fixed an issue in font code generation where compressed fonts could not compile when building with MSVS.
- Fixed an incorrect build configuration for IAR9 Libcpp (C/C++17 runtime) libraries.
- Inserted missing namespace touchgfx in Atomic.hpp.
Enjoy this new version :)