Skip to main content
Associate II
January 14, 2025
Question

ADC: DMA ADC value is not updating after first reading.

  • January 14, 2025
  • 4 replies
  • 866 views

I have configured the ADC in DMA mode to read a single pin for measuring external voltages.
However, I’m encountering an issue where the ADC value is measured correctly on the first call, but on subsequent calls to the function, the ADC value does not get updated. It remains the same regardless of any external voltage applied.

In other words, it only shows the first measured value all the time.

Below is the configuration for the ADC:

Jimit7_0-1736882461393.png

ADC CLK is set to 12MHZ.
Below is the ADC reading function.

void ADC(void)

{

uint16_t ADC_Data;

HAL_ADCEx_Calibration_Start(&hadc1, ADC_SINGLE_ENDED);

HAL_ADC_Start_DMA(&hadc1,(uint32_t*)&ADC_Data ,1);

printf("ADC: %d\n",ADC_Data);

HAL_ADC_Stop_DMA(&hadc1);

}

Thank you,


4 replies

mƎALLEm
Technical Moderator
January 14, 2025

Hello,

Please provide the MCU part number.

See Tips on posting.

Thank you for your understanding.

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."
Jimit7Author
Associate II
January 14, 2025

Hi,

I using stm32wb5mmghtr6 with SDk 1.20.0

Thank you,

Jimit

Jimit7Author
Associate II
January 15, 2025

Is there any update on this?
Thank you,
Jimit

STTwo-32
Technical Moderator
January 30, 2025

Hello @Jimit7 

The STM32WB5MMGH6TR is use an STM32WB MCUs. So, I suggest you have a look at this example and try to migrate it from the NUCLEO board to the STM32WB5MMGH6TR. it should be working fine. After that, you can understand how it works and develop your own example referring to this implementation.

Best Regards.

STTwo-32

Jimit7Author
Associate II
January 30, 2025

Hi STTwo-32,

My code is based on one of the example code from Nucleo board and it does not work for me.

Thank you,

Jimit