Question
ADC on the STM32WL5MOC module not working
- November 25, 2024
- 1 reply
- 515 views
Hi Community!
Currently working with the STM32WL5MOC module on my custom board.
I'm trying to work with the ADC but getting values like the fallowing and not changing even when i connect the ADC signal to ground.
light: 1366
light: 1367
light: 1367
light: 1366
light: 1367
I'm using default configuration for the ADC, and using the STM32cube
this is the code I'm using
while (1)
{
HAL_ADC_Start(&hadc);
HAL_ADC_PollForConversion(&hadc, HAL_MAX_DELAY);
lux = HAL_ADC_GetValue(&hadc);
sprintf(msg, "light: %hu \r\n",lux);
HAL_UART_Transmit(&huart2, (uint8_t *)msg, strlen(msg), HAL_MAX_DELAY);
HAL_Delay(500);
}
Thanks in advance