Skip to main content
Associate II
April 25, 2026
Question

ADC reference for STM32WL31 VBAT measurement

  • April 25, 2026
  • 0 replies
  • 45 views

Good day,

I want to measure the VBAT voltage of a STM32WL31 using its ADC. I setup the ADC channel as follows using the ST HAL driver:

ADC_ChannelConfTypeDef ConfigChannel = {0};
ConfigChannel.Channel = ADC_CHANNEL_VBAT;
ConfigChannel.Rank = ADC_RANK_1;
ConfigChannel.VoltRange = ADC_VIN_RANGE_3V6;
ConfigChannel.CalibrationPoint.Number = ADC_CALIB_POINT_1;
ConfigChannel.CalibrationPoint.Gain = LL_ADC_GET_CALIB_GAIN_FOR_VINMX_3V6();
ConfigChannel.CalibrationPoint.Offset = LL_ADC_GET_CALIB_OFFSET_FOR_VINMX_3V6();
if (HAL_ADC_ConfigChannel(&hadc1, &ConfigChannel) != HAL_OK)
{
 Error_Handler();
}

I seem to be getting correct ADC measurements (actual=3.0V, adc_measured_&_converted=3.15V), but the detail seems to be sparsely documented in the device datasheet and manual, so I just want to check a few things:

 

Q1: I am not sure how the calibration point number relates to the measurement - when would one use ADC_CALIB_POINT_2 etc?

 

Q2: What is the reference voltage used by the ADC? The manual mentions VDDA, which would not make sense measuring VBAT (as they are the same voltage). The ADC reference seems to be 1.2V - is this the internal bandgap voltage also used by the comparator? And what is its voltage tolerance typically?


Q3: As VBAT is defined to be on a negative single ended channel, I'm assuming the raw measurement decreases as VBAT voltage increases? So in order to convert to voltage, it seems:

  1. Take raw, calibrated ADC measurement (e.g. 325)
  2. Convert to voltage (e.g. full-scale is 3.6V, so for 12-bits 325/4096 is 0.285V
  3. Adjust for negative single ended (e.g. 3.6V - 0.285V = 3.315V, which seem in line with the actual applied voltage of 3.30V)

 

Thank you.