B-WL5M-SUBG1, MB1779 board, STM32WL5MOC LoRa device tree clarification
Hello
I have a MB1779 B-WL5M-SUBG1 board that I am trying to adapt some LoRa example code from the Nucleo-WL55JC. I see the LoRa front ends are different and the device tree needs to be modified to work, however the PC5 and PC3 pins are not defined on the data sheet with a reference to the GPIO pin that should be used to communicate with the module. It seems the data sheet reveals Pin 27 as the switch between high and low power.
My question is:
To communicate with the module as on the Nucleo-WL55JC, what would the device tree need to refer to for RX/TX?
This is a new process for me, any help is greatly appreciated.
Thank you
Other relevant posts:
https://community.st.com/t5/stm32-mcus-wireless/b-wl5m-subg1-rf-switch/td-p/737015