cmwx1zzabz_0xx project on B-L072Z-LRWAN1 discovery board: serial console question
I've built cmwx1zzabz_0xx project on B-L072Z-LRWAN1 discovery board. From the source code, it looks like the app configures a 9600 baud serial console using UART1 on the STM32LO72 on the MuRata LoRa module.
Please confirm that the TX/RX signals are available at PA9 and PA10 on the discovery board's pin header.
Which #defines are necessary to route app console logging as well as AT command responses to this console?
Thanks,
Curtis