Develop an application using the STEVAL-25R200A
Hello,
I am exploring the STEVAL-25R200A, and I want to build a pollingTagDetect application, using NFC10A1_PollingTagDetect that comes with the X-CUBE-NFC10 package, in STEVAL-25R200-STM32G0B1.ioc but i can't get it to work.
When i flash the code into the steval, this prints in the com4 port:
Welcome to X-NUCLEO-NFC10A1
Toggling Wake Up mode ON
And that's it, nfc tags are never detected.
I made sure to update the IPs for the ones that STEVAL-25R200-STM32G0B1.ioc includes.

The steval works just fine in ST25R200 EVAL GUI and ST25PC-NFC GUI.
I appreciate your help