Disable Logging WPAN WBA5x
Hello,
I upgraded from CubeIDE 1.17 to 1.18 and from WBA 1.5.0 to 1.6.0 and now I get this error the following error. I have logging disabled in WPAN configuration and no IP selected for logs under platform settings tab.
../Core/Inc/app_conf.h:291:2: error: #error "ERROR : you need to indicate an (LP)UART for the Log on CubeMX."
if I comment out this #error line in aoo_conf.h, I get other errors:
../Projects/Common/WPAN/Interfaces/adv_trace_usart_if.c:73:3: error: 'LOG_UART_HANDLER' undeclared (first use in this function)
So there is some code generated which shouldnt be. There was no problem with this previously.
Best regards