Error: FUS_STATE_IMG_NOT_FOUND
Hi,
Totally newb. I have a custom board with a STM32WB55CEU6. Connected over ST-LINK.
I'm trying to upgrade FUS. Using stm32wb5x_FUS_fw.bin at 0x0807A000
Everything seems to work fine until the very last step, where I get an error: FUS_STATE_IMG_NOT_FOUND: Firmware/FUS upgrade requested but no image found. (such as image header corrupted or flash memory corrupted)
Any ideas?
Here's my log:
16:59:29 : Old Firmware delete ...
16:59:29 : Warning: Option Byte: nSWboot0, value: 0x0, was not modified.
16:59:29 : Warning: Option Byte: nboot0, value: 0x1, was not modified.
16:59:29 : Warning: Option Byte: nboot1, value: 0x1, was not modified.
16:59:29 : Warning: Option Bytes are unchanged, Data won't be downloaded
16:59:29 : Time elapsed during option Bytes configuration: 00:00:00.000
16:59:29 : Succeeded to set nSWboot0=0 nboot1=1 nboot0=1
16:59:29 : Memory Programming ...
16:59:29 : Opening and parsing file: 0x495_FUS_Operator.bin
16:59:29 : File : 0x495_FUS_Operator.bin
16:59:29 : Size : 8.00 KB
16:59:29 : Address : 0x08000000
16:59:29 : Erasing memory corresponding to segment 0:
16:59:29 : Erasing internal memory sectors [0 1]
16:59:29 : Download in Progress:
16:59:29 : File download complete
16:59:29 : Time elapsed during download operation: 00:00:00.212
16:59:29 : Application is running, Please Hold on...
16:59:36 : Reconnecting...
16:59:36 : Reconnected !
16:59:36 : Warning: FUS_STATE_IMG_NOT_FOUND, Flash already empty !
16:59:37 : Firmware delete Success
16:59:37 : Download Stack/FUS image at address 0x807A000 ...
16:59:37 : Memory Programming ...
16:59:37 : Opening and parsing file: stm32wb5x_FUS_fw.bin
16:59:37 : File : stm32wb5x_FUS_fw.bin
16:59:37 : Size : 424.79 KB
16:59:37 : Address : 0x0807A000
16:59:37 : Erasing memory corresponding to segment 0:
16:59:37 : Erasing internal memory sectors [122 228]
16:59:39 : Download in Progress:
16:59:46 : File download complete
16:59:46 : Time elapsed during download operation: 00:00:08.449
16:59:46 : Firmware Upgrade process started ...
16:59:46 : Application is running, Please Hold on...
17:00:18 : Reconnecting...
17:00:18 : Reconnected !
17:00:18 : Error: FUS_STATE_IMG_NOT_FOUND: Firmware/FUS upgrade requested but no image found. (such as image header corrupted or flash memory corrupted)