Error in STM32WL5MOC User Manual (UM3127, rev 3, Jan 2025)
There is an error in table 17 on page 33 in regards to two of the pin positions for the MB1880A adapter. Table 17 states that pin 2 is SPI1_MOSIP (PA7) / UART1_TX (PC1) and pin 3 is SPI1_MISOP (PA6) / UART1_RX (PC0). These two pins are reversed in both the CN2 and CN3 columns.
In actuality, pin 2 is SPI1_MOSIP (PA7) / UART1_RX (PC0) and pin 3 is SPI1_MISOP (PA6) / UART1_TX (PC1).
This is confirmed by table 13 (page 28), the MB1779 schematic (MB1779-HIGH-BAND-B02 Board schematic under the B-WL5M-SUBG1 CAD Resources tab), and wasting an hour trying to determine why the I2C3 port was not talking to a device.