Flash Erase Operation Stuck During BLE Scanning on STM32WB55
Dear ST Support,
I am using the STM32WB55 series and have encountered an issue where the Flash erase operation gets stuck when BLE scanning is active. Specifically, the Flash erase call (SHCI_C2_FLASH_EraseActivity(ERASE_ACTIVITY_ON)) does not proceed as long as the BLE scan procedure is running, even if the scan interval and window are configured with minimal values (e.g., SCAN_P = 0x320 and SCAN_L = 0x10). It seems that as long as BLE scanning is ongoing, the Flash operation remains blocked.
From my understanding, the BLE stack on the M0 core occupies some resources during the scan procedure, and Flash operations are blocked until all BLE activities are terminated. This behavior persists even when BLE is only actively scanning for a small portion of the interval.
Could you please clarify:
- Is it expected that Flash erase/write operations cannot be performed during any ongoing BLE activity, regardless of scan interval/window settings?
- Is there a recommended method to safely perform Flash operations when BLE scanning is required, without stopping BLE completely?
Thank you for your support.