FUS,BLE update
FUS and BLE update.
I would like to know if it is possible to update FUS (1.2.0)(2.1.0) and BLE (1.23.0) via SWD. I need to update two boards simultaneously and am having problems with programming via DFU. One of the boards always shows an error. I usually program one board at a time, and before, I only updated BLE without updating FUS, and everything worked correctly via SWD. Now that I need to update FUS and BLE simultaneously, an error occurs. Is it possible to perform this update, or can I only do it via DFU (it works with one board, but with two, one of them always shows an error)? What is the best way to perform this update? I use the CLI with a script to write, I think it's faster.
Edited by Moderator to comply with the community rules.
Please use the English language as it is an international community, ensuring that all Community users can understand your post.