Skip to main content
MSing.1713
Associate III
October 23, 2025
Question

How do we enable BLE scanning on STM32WB5x?

  • October 23, 2025
  • 1 reply
  • 184 views

This is a repost because the forum decided that my follow-up was a 'solution'.

We want to scan using the BLE Full stack, v1.21.  What is happening is that the BLE stack is claiming that these HCI commands are unsupported. 

HCI_LE_SetScan_Parameters
HCI_LE_SetScan_Enable
HCI_LE_Set_Extended_Scan_Parameters
HCI_LE_Set_Extended_Scan_Enable
HCI_Read_Local_Supported_Commands

The last one is unexpected.

The AN5270 doesn't list the 'full' stack among the firmware that is documented as having specific commands.  Section 2.1:

In Table 1 "Y" means that the corresponding command applies to the dedicated Bluetooth® Low Energy (BLE) stack variant, namely LO / BO / PO / BF / LB, respectively, for Link layer only / Beacon only / Peripheral only / Basic feature / Link layer only basic.

Is there another place for documentation on the supported HCI commands per stack?  Is there another set of commands we should be used to enable scanning?

Cheers

1 reply

MSing.1713
Associate III
October 23, 2025

I have made some progress.

The ACI/HCI documentation is, to be blunt, pretty terrible.  The most difficult problem is that it lists a lot of commands that are not available on the STM32WB55x full-ble stack without providing any information about their presence or absence.

The ACI_Reset command looks to be universal, but it isn't supported.

The HCI Central scanning commands don't appear to be support.  But, the ACI_GAP_Start_General_Discovery is.  This is the first thing that worked.

https://community.st.com/t5/stm32-mcus/how-to-configure-the-stm32wb-le-central-client-or-peripheral/ta-p/49375

The above article is helpful in a schematic way.    It would have been nice for this article to include source code or better yet, for there to be source code in the examples that implements this behavior.

Hey, ST!  Can you do something about the explanations of which commands are available in which firmware load?