How to pass CAN bus data to the BLE stack using the sequencer?
Hello, I have a STM32WB55RE connected to a CAN bus. I'm receiving the CAN data via the Main function using polling. When a message is received (250K Baud Rate) I want to forward that data to the BLE stack so I can send it to another STM32WB55RE. I'm currently using the sequencer to manage all the BLE tasks. There doesn't seem to be any queue or semaphore that I can use with the sequencer.
Is there a preferred method to CAN bus data from the Main loop to a task running within the sequencer?
Kindest regards.