How to use USART2 instead of USART1 in BLE_p2pServer example?
Hi
I am using the BLE_p2pServer example with NUCLEO-WBA55 and want to use USART2 instead of USART1. If I use USART1 and send a byte via HTerm, the task UTIL_SEQ_SetTask( 1<<CFG_TASK_SEND_NOTIF_ID, CFG_SEQ_PRIO_0); should be executed as soon as an RxCpltCallback event (in file usart_if.c) is triggered.
static void UsartIf_RxCpltCallback(UART_HandleTypeDef *huart)
{
/* USER CODE BEGIN UsartIf_RxCpltCallback 1 */
UTIL_SEQ_SetTask( 1<<CFG_TASK_SEND_NOTIF_ID, CFG_SEQ_PRIO_0);
/* USER CODE END UsartIf_RxCpltCallback 1 */
RxCpltCallback(&charRx, 1, 0);
HAL_UART_Receive_IT(&huart1, &charRx, 1);
/* USER CODE BEGIN UsartIf_RxCpltCallback 2 */
/* USER CODE END UsartIf_RxCpltCallback 2 */
}When I establish a BLE connection with the “nRF Connect” app, I receive the corresponding notification (Same effect as when I press button1)

and I also receive the corresponding logs via HTerm.

But if I now change “serial links for logs” to USART2 and configure USART2 exactly the same as USART1, I get confused characters as log information like this: