Skip to main content
DavePfz
Associate III
December 16, 2025
Solved

Implementing BLE SPP protocol

  • December 16, 2025
  • 3 replies
  • 690 views

I have a requirement to implement the BLE SPP protocol that will eventually be ported to the STM32WB1MCC module. Since I am totally new to BLE, I'd like a recommendation for a place to start. Specifically which demo or eval board and associated software. For example, is the NUCLEO-WB51CC the best (most supported and easily ported)?

Thanks, Dave

Best answer by Andrew Neil

There is no such thing as SPP (Serial Port Profile) in BLE - it is purely a Bluetooth "Classic" Profile.

See:

https://community.st.com/t5/stm32-mcus-wireless/bluetooth-classic-profiles-spp-a2dp-on-stm32wb/m-p/253911/highlight/true#M10614

 

PS:

Don't forget to visit the pinned post, Please go and visit our wiki pages to support your projects on our wireless product families - it has links to introductory stuff for BLE on STM32 ...

3 replies

Andrew Neil
Andrew NeilBest answer
Super User
December 16, 2025

There is no such thing as SPP (Serial Port Profile) in BLE - it is purely a Bluetooth "Classic" Profile.

See:

https://community.st.com/t5/stm32-mcus-wireless/bluetooth-classic-profiles-spp-a2dp-on-stm32wb/m-p/253911/highlight/true#M10614

 

PS:

Don't forget to visit the pinned post, Please go and visit our wiki pages to support your projects on our wireless product families - it has links to introductory stuff for BLE on STM32 ...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
DavePfz
DavePfzAuthor
Associate III
December 16, 2025

OK. So I used the wrong term. Shows how totally new I am to BLE!

So, following the link, what I want is "BLE_CableReplacement"

Noting that the thread is now six years old and that the links included lead to additional problems by others, is the NUCLEO-WB51CC still the best starting point? (From past experience, I'm guessing there may be a newer board available.)

Thanks, Dave

StevenG
Associate III
December 16, 2025

I haven't heard of the NUCLEO-WB51CC but I would suggest NUCLEO-WB55RG.  It is supported (partially) in Zephyr and works with STM32CubeIDE reference designs.

 

The Zephyr sample project peripheral_nus implements the Nordic UART Serial protocol which is essentially BLE cable replacement.

 

The STM32WB55 has 1MB Flash / 256k SRAM vs the STM32WB15's 320K Flash / 48K SRAM.  I would suggest starting with the larger part and seeing if your project can fit into the smaller part at a later date.