Skip to main content
Associate
February 2, 2025
Question

Inquiry About STM32WLE5C8U6 for 915 MHz LoRaWAN End Node Development

  • February 2, 2025
  • 1 reply
  • 414 views

Hello,

I am planning to develop a 915 MHz LoRaWAN end node using the STM32WLE5C8U6. My goal is to send data from several sensors—such as GNSS, temperature, and accelerometer—directly to a gateway without employing an external MCU.

1- Could you please advise if the integrated MCU in the STM32WLE5C8U6 is sufficient for handling these tasks?

2- I intend to use a chip antenna (0915AT43A0026001E) and would like to know if it is feasible to achieve a 10 km range in a rural open area with this setup.

3- would you recommend a 4-layer or 6-layer PCB for this application?

Thank you in advance for your assistance.

Best regards,

1 reply

STTwo-32
Technical Moderator
February 2, 2025

Hello @jackob @and welcome to the ST Community.

1- Yes, you can use one of the STM32WLE MCUs for such a project but you need just to make sure you have enought peripherals and pins for all your sensors. On this,  DS13105 should help you.

2- About this antenna, i didn’t tested personally but i can tel you that 10KM is possible with a good antenna. For that, you can ask a RF expert. Hi should be able to help you.

3- For the number of layers, it depends on lots of conditions. So, you may need to ask for some guidance from a HW expert. You can also have a look at this video that should help you with some design tips.

Best Regards.

STTwo-32