Associate
March 3, 2025
Question
Linking errors of examples with new STM32WBA release 1.6 & Cannot launch debugger in VS Code
- March 3, 2025
- 2 replies
- 567 views
Hello there,
I am trying to get my Nucleo WBA55 running with the new CubeMX 6.14 and the new MCU package 1.6.0.
Generating a project with just the bare minimum BLE GATT Server application, CMake configuration.
Importing into VS Code with extension 2.1.1, compiling "debug" version, I get several multiple definition errors.
The file is included twice in the makefiles in two different sections it seems.
[build] [86/86] Linking C executable LCU_Demo.elf
[build] FAILED: LCU_Demo.elf
[build] C:\Windows\system32\cmd.exe /C "cd . && C:\ST\STM32CubeCLT_1.17.0\GNU-tools-for-STM32\bin\arm-none-eabi-gcc.exe -mcpu=cortex-m33 -mfpu=fpv4-sp-d16 -mfloat-abi=hard -Wall -Wextra -Wpedantic -fdata-sections -ffunction-sections -mcpu=cortex-m33 -mfpu=fpv4-sp-d16 -mfloat-abi=hard -Wall -Wextra -Wpedantic -fdata-sections -ffunction-sections -mcpu=cortex-m33 -mfpu=fpv4-sp-d16 -mfloat-abi=hard -Wall -Wextra -Wpedantic -fdata-sections -ffunction-sections -O0 -g3 -mcpu=cortex-m33 -mfpu=fpv4-sp-d16 -mfloat-abi=hard -T "C:/SVN/LasGAR2/Demonstrator/Software/Source/_trunk_/Nucleo-WBA/SUT/LCU_Demo/STM32WBA55xx_FLASH.ld" --specs=nano.specs -Wl,-Map=LCU_Demo.map -Wl,--gc-sections -Wl,--start-group -lc -lm -Wl,--end-group -Wl,--print-memory-usage @CMakeFiles\LCU_Demo.rsp -o LCU_Demo.elf && cd ."
[build] C:/ST/STM32CubeCLT_1.17.0/GNU-tools-for-STM32/bin/../lib/gcc/arm-none-eabi/12.3.1/../../../../arm-none-eabi/bin/ld.exe: CMakeFiles/LCU_Demo.dir/Projects/Common/WPAN/Startup/stm32wbaxx_ResetHandler_GCC.s.obj: in function `backup_loop_init':
[build] C:/SVN/LasGAR2/Demonstrator/Software/Source/_trunk_/Nucleo-WBA/SUT/LCU_Demo/Projects/Common/WPAN/Startup/stm32wbaxx_ResetHandler_GCC.s:132: multiple definition of `backup_system_register'; cmake/stm32cubemx/CMakeFiles/Startup.dir/__/__/Projects/Common/WPAN/Startup/stm32wbaxx_ResetHandler_GCC.s.obj:C:/SVN/LasGAR2/Demonstrator/Software/Source/_trunk_/Nucleo-WBA/SUT/LCU_Demo/Projects/Common/WPAN/Startup/stm32wbaxx_ResetHandler_GCC.s:132: first defined here
[build] C:/ST/STM32CubeCLT_1.17.0/GNU-tools-for-STM32/bin/../lib/gcc/arm-none-eabi/12.3.1/../../../../arm-none-eabi/bin/ld.exe: CMakeFiles/LCU_Demo.dir/Projects/Common/WPAN/Startup/stm32wbaxx_ResetHandler_GCC.s.obj: in function `restore_loop_init':
[build] C:/SVN/LasGAR2/Demonstrator/Software/Source/_trunk_/Nucleo-WBA/SUT/LCU_Demo/Projects/Common/WPAN/Startup/stm32wbaxx_ResetHandler_GCC.s:158: multiple definition of `restore_system_register'; cmake/stm32cubemx/CMakeFiles/Startup.dir/__/__/Projects/Common/WPAN/Startup/stm32wbaxx_ResetHandler_GCC.s.obj:C:/SVN/LasGAR2/Demonstrator/Software/Source/_trunk_/Nucleo-WBA/SUT/LCU_Demo/Projects/Common/WPAN/Startup/stm32wbaxx_ResetHandler_GCC.s:158: first defined here
[build] C:/ST/STM32CubeCLT_1.17.0/GNU-tools-for-STM32/bin/../lib/gcc/arm-none-eabi/12.3.1/../../../../arm-none-eabi/bin/ld.exe: CMakeFiles/LCU_Demo.dir/Projects/Common/WPAN/Startup/stm32wbaxx_ResetHandler_GCC.s.obj: in function `Reset_Handler':
[build] C:/SVN/LasGAR2/Demonstrator/Software/Source/_trunk_/Nucleo-WBA/SUT/LCU_Demo/Projects/Common/WPAN/Startup/stm32wbaxx_ResetHandler_GCC.s:79: multiple definition of `Reset_Handler'; cmake/stm32cubemx/CMakeFiles/Startup.dir/__/__/Projects/Common/WPAN/Startup/stm32wbaxx_ResetHandler_GCC.s.obj:C:/SVN/LasGAR2/Demonstrator/Software/Source/_trunk_/Nucleo-WBA/SUT/LCU_Demo/Projects/Common/WPAN/Startup/stm32wbaxx_ResetHandler_GCC.s:79: first defined here
[build] C:/ST/STM32CubeCLT_1.17.0/GNU-tools-for-STM32/bin/../lib/gcc/arm-none-eabi/12.3.1/../../../../arm-none-eabi/bin/ld.exe: CMakeFiles/LCU_Demo.dir/Projects/Common/WPAN/Startup/stm32wbaxx_ResetHandler_GCC.s.obj: in function `CPUcontextSave':
[build] C:/SVN/LasGAR2/Demonstrator/Software/Source/_trunk_/Nucleo-WBA/SUT/LCU_Demo/Projects/Common/WPAN/Startup/stm32wbaxx_ResetHandler_GCC.s:109: multiple definition of `CPUcontextSave'; cmake/stm32cubemx/CMakeFiles/Startup.dir/__/__/Projects/Common/WPAN/Startup/stm32wbaxx_ResetHandler_GCC.s.obj:C:/SVN/LasGAR2/Demonstrator/Software/Source/_trunk_/Nucleo-WBA/SUT/LCU_Demo/Projects/Common/WPAN/Startup/stm32wbaxx_ResetHandler_GCC.s:109: first defined here
[build] C:/ST/STM32CubeCLT_1.17.0/GNU-tools-for-STM32/bin/../lib/gcc/arm-none-eabi/12.3.1/../../../../arm-none-eabi/bin/ld.exe: warning: C:/ST/STM32CubeCLT_1.17.0/GNU-tools-for-STM32/bin/../lib/gcc/arm-none-eabi/12.3.1/thumb/v8-m.main+fp/hard/crtn.o: missing .note.GNU-stack section implies executable stack
[build] C:/ST/STM32CubeCLT_1.17.0/GNU-tools-for-STM32/bin/../lib/gcc/arm-none-eabi/12.3.1/../../../../arm-none-eabi/bin/ld.exe: NOTE: This behaviour is deprecated and will be removed in a future version of the linker
[build] Memory region Used Size Region Size %age Used
[build] RAM: 43840 B 128 KB 33.45%
[build] FLASH: 282384 B 1 MB 26.93%
[build] collect2.exe: error: ld returned 1 exit status
[build] ninja: build stopped: subcommand failed.
[proc] The command: C:/ST/STM32CubeCLT_1.17.0/CMake/bin/cmake.exe --build C:/SVN/LasGAR2/Demonstrator/Software/Source/_trunk_/Nucleo-WBA/SUT/LCU_Demo/build/Debug -- exited with code: 1
[driver] Build completed: 00:00:08.214
[build] Build finished with exit code 1When I delete one of the occurrences in the CMakeLists.txt it links correctly.
The second error I could not get rid of: when clicking on "run" in VS Code, Windows asks me what should it do with a ELF file. Any idea of what went wrong?