Skip to main content
Associate II
October 9, 2025
Solved

LoRaWAN Software Stack for STM32WLE5xx

  • October 9, 2025
  • 1 reply
  • 252 views

How I get the software stack/firmware library stack with LoRaWAN for STM32WLE5xx MCU (other than Seed Studio Library) ?. In github, stm32wl repository only has a STM32WL55JC drivers alone. Is there any possibilities to get a firmware stack for STM32WLE5xx ? If anyone have an idea kindly let me know.

Best answer by Imen.D

Hello @mathi_manoj and welcome to the Community,

STM32CubeWL supports all STM32WL MCUs. However, examples and BSP files are available only for the NUCLEO-WL55JC board and the B-WL5M-SUBG1, which are the official STM32WL evaluation boards.

There is no evaluation board based on the STM32WLE. If you have an evaluation board based on the STM32WLE, I recommend you contacting the board or module manufacturer for additional support.

1 reply

Imen.DBest answer
Technical Moderator
October 9, 2025

Hello @mathi_manoj and welcome to the Community,

STM32CubeWL supports all STM32WL MCUs. However, examples and BSP files are available only for the NUCLEO-WL55JC board and the B-WL5M-SUBG1, which are the official STM32WL evaluation boards.

There is no evaluation board based on the STM32WLE. If you have an evaluation board based on the STM32WLE, I recommend you contacting the board or module manufacturer for additional support.

"When your question is answered, please close this topic by clicking ""Accept as Solution"".ThanksImen"