Skip to main content
Associate
April 2, 2026
Question

MTU Size Limitation on BLE (BlueNRG-M0+) – Unable to Send Payload >20 Bytes

  • April 2, 2026
  • 1 reply
  • 170 views

Hello,

I am working with the following setup:

  • Board: B-L4S5I-IOT-01A
  • MCU: STM32L4S5VIT6
  • BLE Module: BlueNRG-M0+ (in built in the Kit)

I am currently facing an issue related to the BLE MTU (Maximum Transmission Unit) size. By default, the payload length is limited to 20 bytes, which is insufficient for my application, as my data length exceeds 180 bytes.

I would like to know:

  • Is there a way to increase the MTU size on the BlueNRG-M0+?
  • Can this be achieved without modifying my existing data transmission mechanism (i.e., without manually fragmenting the data into smaller packets)?

My goal is to transmit larger data packets in a single operation, if supported.

Any guidance or recommended approach would be highly appreciated.

Thank you.

1 reply

Technical Moderator
April 21, 2026

Hello @DdAz ,

The BlueNRG-M0 Bluetooth LE stack supports the default ATT_MTU value (23 bytes). Therefore, this value cannot be increased.

"When your question is answered, please close this topic by clicking ""Accept as Solution"".ThanksImen"