Nucleo STM32WB55RG BLE with Zephyr Project HCI issue
Hi ST community,
I wanted to develop BLE application using the nucleo stm32wb55rg and the zephyr project v4.3.0. what i did is take a nucleo stm32wb55rg board first i upgraded the FUS from the STM32Cube/Repository/STM32Cube_FW_WB_V1.23.0/Projects/STM32WB_Copro_Wireless_Binaries/STM32WB5x/stm32wb5x_FUS_fw_1_2_0.bin
then after this i updated the wireless stack firmware with this one STM32Cube/Repository/STM32Cube_FW_WB_V1.23.0/Projects/STM32WB_Copro_Wireless_Binaries/STM32WB5x/stm32wb5x_BLE_HCILayer_extended_fw.bin.
after this i power cycle the board, which is required for the wireless stack to load.
after that i build a sample from the zephyr v4.3.0 buluetooth samples "Peripheral_dis sample"
i build it for the nucleo_wb55rg board and flash it, the flash logs can be seen below.
after this i connected a serial terminal to view the logs and the logs can be seen below. the zephyr is unable to communicate with the wireless stack with error timeout.
i have tested this setup with multiple wireless stack binaries such is from 1.13.0 and 1.17.0 and 1.19.0 wireless binaries but all resulted in the same error.
what i want is an guide to get started with, or may be look at my current flow and tell me where am i going wrong.
looking forward to hear from you.
thanks and regards
Akbar Shah
*** Booting Zephyr OS build v4.3.0-rc2-127-gf2428c68ff2f ***
ASSERTION FAIL [err == 0] @ WEST_TOPDIR/zephyr/subsys/bluetooth/host/hci_core.c:504
Controller unresponsive, command opcode 0xfc0c timeout with err -11
r0/a1: 0x00000003 r1/a2: 0x08010dfc r2/a3: 0x00000000
r3/a4: 0x00000003 r12/ip: 0x00000000 r14/lr: 0x08002a7b
xpsr: 0x21000000
Faulting instruction address (r15/pc): 0x08002a8a(.venv) flash@Ghost:~/zephyrproject/peripheral_dis$ west flash
-- west flash: rebuilding
ninja: no work to do.
-- west flash: using runner stm32cubeprogrammer
-------------------------------------------------------------------
STM32CubeProgrammer v2.21.0
-------------------------------------------------------------------
ST-LINK SN : 0674FF524957787187011712
ST-LINK FW : V2J39M27
Board : NUCLEO-WB55RG
Voltage : 3.24V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x495
Revision ID : Rev X
Device name : STM32WB5x/35xx
Flash size : 1 MBytes
Device type : MCU
Device CPU : Cortex-M4
BL Version : 0xD5
Debug in Low Power mode enabled
Opening and parsing file: zephyr.hex
Memory Programming ...
File : zephyr.hex
Size : 71.07 KB
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 17]
Download in Progress:
[==================================================] 100%
File download complete
Time elapsed during download operation: 00:00:01.704
RUNNING Program ...
Address: : 0x8000000
Application is running, Please Hold on...
Start operation achieved successfully
(.venv) flash@Ghost:~/zephyrproject/peripheral_dis$