Skip to main content
Associate II
June 19, 2025
Solved

NUCLEO-WB55RG board FW update

  • June 19, 2025
  • 3 replies
  • 1353 views

Hello, 

I have recently started getting familiarized with the P-NUCLEO-WB55 kit, and I have run to my first big mess up. I was attempting to perform a wireless stack FUS routine over the STLink interface, and I might have set a wrong start address for the FUS_fw.bin file (which I have updated to v 2.00). Hence, it seems that I can no longer do a firmware update over the stlink. 

 

The other main issue that I am also facing is that I cannot seem to get the board to boot up to DFU mode. I have tried the dongle, and it boots to DFU mode normally after toggling the switch. However, and correct me if I am wrong, If I follow the procedure outlined here: https://visualgdb.com/tools/STM32WBUpdater/connecting/ , I should be able to boot into DFU mode in the development board. Yet, it does not work.

 

If this is salvageable, I would greatly appreciate any help/support you can provide.

 

Thanks

 

 

Best answer by STTwo-32

Hello All,

This behavior has been solved on the last update of the STM32CubeWB (V1.23.0) using the FUS V2.1.0.

Best Regards.

STTwo-32

3 replies

RobK1
Associate II
June 19, 2025

I found that in my P-NUCLEO-WB55 kit, the Boot select bits in the Option Bytes were not correctly set.

This works for me to boot up in DFU mode:

RobK1_0-1750331527301.png

 

Associate II
June 19, 2025

You are a life-saver, thank you for that.

 

Now I can boot into DFU mode normally. 

Associate II
June 19, 2025

Hello, 

The DFU mode issue is fixed now, but I cannot seem to be able of reflashing the binaries of the wireless stack. Here is what I tried doing:

 

1- I did a firmware delete

2- I am now trying to reflash each part of the wireless correctly starting with the FUS binary, but I am not able of flashing anything, here is an example log I get:

15:32:15 : UR connection mode is defined with the HWrst reset mode
15:32:15 : USB speed : Full Speed (12MBit/s)
15:32:15 : Manuf. ID : STMicroelectronics
15:32:15 : Product ID : DFU in FS Mode
15:32:15 : SN : 207431743831
15:32:15 : DFU protocol: 1.1
15:32:15 : Board : --
15:32:15 : Device ID : 0x0495
15:32:15 : UPLOADING OPTION BYTES DATA ...
15:32:15 : Bank : 0x00
15:32:15 : Address : 0x1fff8000
15:32:15 : Size : 128 Bytes
15:32:15 : UPLOADING ...
15:32:15 : Size : 4 Bytes
15:32:15 : Address : 0x1FFF8070
15:32:15 : Read progress:
15:32:15 : Data read successfully
15:32:15 : Time elapsed during the read operation is: 00:00:00.002
15:32:15 : UPLOADING ...
15:32:15 : Size : 1024 Bytes
15:32:15 : Address : 0x8000000
15:32:15 : Read progress:
15:32:15 : Data read successfully
15:32:15 : Time elapsed during the read operation is: 00:00:00.004
15:32:19 : FUS state is FUS_IDLE
15:32:19 : FUS status is FUS_NO_ERROR
15:32:21 : Deleting firmware ...
15:32:22 : Firmware delete finished
15:32:22 : Firmware delete execution finished
15:32:32 : FUS state is FUS_ERROR
15:32:32 : FUS status is FUS_IMAGE_NOT_FOUND
15:32:34 : FUS state is FUS_IDLE
15:32:34 : FUS status is FUS_NO_ERROR
15:32:37 : Old Firmware delete ...
15:32:37 : Deleting firmware ...
15:32:37 : Firmware delete finished
15:32:37 : FUS state is FUS_ERROR
15:32:37 : FUS status is FUS_IMAGE_NOT_FOUND
15:32:40 : FUS state is FUS_IDLE
15:32:40 : FUS status is FUS_NO_ERROR
15:32:42 : Download Stack/FUS image at address 0x80EE000 ...
15:32:42 : Opening and parsing file: stm32wb5x_FUS_fw.bin
15:32:42 : Memory Programming ...
15:32:42 : File : stm32wb5x_FUS_fw.bin
15:32:42 : Size : 23.89 KB
15:32:42 : Address : 0x080EE000
15:32:42 : Erasing memory corresponding to sector 0:
15:32:42 : Erasing internal memory sectors [238 243]
15:32:43 : Download in Progress:
15:32:43 : failed to download Sector[0]
15:32:43 : failed to download the File
15:32:43 : Failed to download image!
15:32:43 : Connection to device 0x495 is lost
15:32:43 : Disconnected from device.

 

STTwo-32
Technical Moderator
June 19, 2025

Hello @majidsurefow 

Could you please state the exact steps (with screenshots if possible) on how you have done this update. and a final screenshot similar to this one: 

STTwo32_0-1750334576264.png

Best Regards.

STTwo-32

Associate II
June 19, 2025

Hello, 

 

Thanks for your reply.

 

I am currently using Firmware 2.0.3

Here is a screenshot of what I get if I am using the DFU-USB Interface to check the FUS status:

majidsurefow_1-1750335979729.png

I am currently using FUS 2.0.0.3 as I have installed it blindly while trying to upgrade my BLE/ZigBee binary. The STM32WB_Copro_Wireless_Binaries directory I am using is the one that results from cloning the https://github.com/STMicroelectronics/STM32CubeWB/tree/master  repo. 

Here is a screenshot of what I have after deleting the firmware:

 

majidsurefow_3-1750336196074.png

I am setting the starting Address to 0x080EE000 as stated in the release notes, and attempting to flash the FUS binary:

 

majidsurefow_4-1750336634313.png

 

Next, I tried flashing a random file which was the stm32wb5x_BLE_HCILayer_fw.bin:

majidsurefow_6-1750337537643.png

This is the only one that flashes correctly. If I try to flash something else, lets say stm32wb5x_BLE_Zigbee_FFD_static_fw.bin, here is what I get:

majidsurefow_9-1750338832553.png

The device disconnects mid-flash, and I have reconnect it using the GUI option.

 

 

 

 

 

 

 

STTwo-32
STTwo-32Best answer
Technical Moderator
August 1, 2025

Hello All,

This behavior has been solved on the last update of the STM32CubeWB (V1.23.0) using the FUS V2.1.0.

Best Regards.

STTwo-32