NUCLEO WL55JC1 - No device found on target on STM32CubeIDE
Hi,
I recently bought two NUCLEO-WL55JC1 boards and was testing the SubGHz_Phy_PingPong example to establish communication between them. Everything was working fine at first, but at some point (I’m not sure if I changed anything), one of the boards stopped being recognized by STM32CubeIDE when trying to debug.
The error message is:
"Target no device found. Error in initializing ST-LINK device. Reason: No device found on target."
When I connect the board to the PC via USB, it is detected, but a FAIL.TXT file appears with the message:
"The interface firmware FAILED to reset/halt the target MCU".
I know the firmware is still loaded because, when powered, this board still sends messages that are received by the other one (which works normally).
The jumpers on both boards are configured the same way, and I have tried debugging through both USB and SWD without success.
Is there a way to make STM32CubeIDE detect the board again? What could be the cause of this issue?
Thanks in advance for your support.