NUCLEO-WL55JC1 Sleep Mode Current Consumption
Hi,
I am using the NUCLEO-WL55JC1 board and referring to the PWR_STOP2_RTC example to measure current consumption.
I have isolated the ST-LINK section and am powering the board with an external 3.6 V supply for accurate measurement. However, in sleep (STOP2) mode, the measured current consumption is about 1.64 mA, which seems higher than expected.
Please let me know if this is normal for this configuration or if any additional steps are required to further reduce the current consumption.