openocd is not working with STM32WBA65 CPU
The bottom line is the "wba" file stm32wbax.cfg is missing from openocd
Here are the details:
- I have designed a board with the STM32WBA65 CPU.
- I downloaded openocd
- Downloading from origin https://github.com/STMicroelectronics/OpenOCD.git (fetch)
- git checkout v0.12.0-rc3
- But the needed file stm32wbax.cfg is missing
- find . -name "stm32wb*"
./tcl/target/stm32wbx.cfg
- find . -name "stm32wb*"
What I need is an openocd that works with the stm32wbax.cfg file.
I have found the file in https://github.com/openocd-org/openocd
However, that file does not work with openocd distributed by MorseMicro
- openocd --version
xPack Open On-Chip Debugger 0.12.0+dev-01312-g18281b0c4-dirty (2023-09-04-22:31
And I built openocd from scratch and it also fail
- openocd --version
Open On-Chip Debugger 0.12.0-rc3-00999-gfcb40f49b (2025-08-05-13:39)
Conclusion:
When you find the file stm32wbax.cfg, please make sure it works with openocd.
And please add LABELS to your GUI so I can file under STM32WBA or STM32WBA65