P2P_Client needs to be placed in bootloader mode after executing
Hello;
I am very new to STM32 products. I have been working with the P2P_Server and P2P_client examples using the STM32WB05KZV6TR MCU.
As I use the P2P_clent example in both the Nucleo board WB05KZ and a custom board and load the built image, the next time I try to download a new image I need to put the nucleo board into Bootloader mode(BOOT0 jumped to Vcc) and download the new image that way. The custom board that I am working with currently has no hardware way of putting it into bootloader mode therefore I cannot load a new image.
My question is, why do I need to put the nucleo board into bootloader mode to load an P2P_Client image?, The P2P_server does not have this issue
Is there a way to prevent this?
thanks
Fernando